We understand that energy efficiency and plant reliability are of crucial importance to any hospital engineering function, as strict targets have to be met and downtime must be minimised.
Our range of products and solutions is designed to maximise the efficiency of your steam system from the boilerhouse throughout the distribution system to the condensate recovery system.
Achieve consistent and reliable sterilisation every time by using the right steam quality
Spirax EasiHeat™
Some of the areas where we can provide help include:
Our technical experts can also offer specialist advice and products to improve the performance and reliability of specific steam-using applications such as:
"Our decision to upgrade to the EasiHeat systems was an easy one to make – we knew they would be perfect for this project."Brian Colley, Energy & Environmental Engineer at Leighton Hospital View Case Study
The CSF16 steam filter is a horizontal, in-line high efficiency filter used to remove contaminate particles from steam.
A range of automatic boiler water TDS control systems which constantly monitor the TDS level of the boiler water and blowdown when necessary.
The SPIRA-TROL range of two port single seat globe valves with cage retained seats is available in a range of materials and sizes up to DN100 / 4". EN or ASME/ANSI.
Heat exchanger upgrade cuts Leighton Hospital’s water heating costs by 15%.
Clean steam generators boosts steam quality standards at Waterford Regional Hospital.
Switching to EasiHeat delivers 15% energy savings at Aberdeen Royal Infirmary.
Plate heat exchangers from Spirax Sarco are saving energy, reducing maintenance costs and improving the comfort of patients at Leighton Hospital.
Synergy Health in Sheffield, has reduced gas consumption in its boiler by 11% thanks to an innovative heat recovery system from Spirax Sarco.
If you were asked what the biggest sources of greenhouse gas emissions were, it's unlikely that the world's healthcare system would be high up the list. But that's not the case. Being something that's universally needed, it has a significant impact.
The upgrade to Spirax Sarco’s EasiHeat™ steam-to-hot-water solutions and Reverse Osmosis (RO) system in ten plant rooms helped this acute hospital reduce energy and maintenance costs.
Your Guide to achieving reliable high-quality sterilisation through the provision of dry clean steam.
Members of The Institute of Healthcare Engineering and Estate Management (IHEEM) will now be able to take advantage of industry-leading training for steam systems as part of a new partnership.
The supply of a new, energy-saving heating and hot water system for Kettering General Hospital, played a critical role in getting government funding for the project.
Noble’s Hospital laundry is saving more than £14,500 a year in energy, water and treatment chemicals, thanks to the installation of a FREME system.