It’s a question we hear more and more: “Can I reduce the pressure of my steam boiler?”
The short answer is, “Yes, you can”—but the real question is: should you? While reducing boiler pressure might seem like a simple way to lower energy consumption and CO₂ emissions, the reality is more complex. Let’s explore the implications, dispel some myths, and highlight better strategies for optimising your steam system, all with the support of Spirax Sarco’s Advance Consulting service.
Why Consider Reducing Boiler Pressure?
The primary drivers behind this question often include:
On the surface, it seems logical: if you’re generating steam at a high pressure (e.g., 10 BarG) but only need 2 BarG at the point of use, why not generate steam at 5 BarG instead? You’d burn less fuel, right?
Not necessarily. The latent heat content of lower-pressure steam is also reduced. This means your boiler might need to produce a greater mass of steam to meet process demands, potentially offsetting any perceived savings.
Why Reducing Boiler Pressure May Cause More Problems
Here’s why reducing your boiler pressure might not be the best move:
1. Reduced Resilience
At higher pressures, boiler water contains more sensible heat, acting as an energy buffer during periods of high demand. Lowering the pressure reduces this stored energy, potentially leading to:
2. Infrastructure Mismatch
Your current steam system is likely designed for the original pressure and flow rate. Reducing pressure can cause:
3. Safety and Control Issues
4. Poor Steam Quality
Lower-pressure steam has larger bubbles, leading to:
5. Steam Trap Inefficiencies
Steam traps are designed for a specific condensate load and pressure drop. A reduction in boiler pressure can lead to:
A Better Approach: Optimise, Don’t Compromise
If your goal is to reduce fuel consumption and CO₂ emissions, reducing boiler pressure isn’t your only—or best—option. Greater savings, with far less disruption, can often be found elsewhere in the steam and condensate loop.
Here’s how Spirax Sarco’s Advance Consulting service can help:
1. Optimise Your System
2. Improve Maintenance and Monitoring
3. Upgrade Technology
The Spirax Sarco Philosophy: Keep It Designed for Purpose
Boiler pressure should generally remain at its original design conditions. Changes can disrupt your system, creating more problems than they solve. Instead, focus on holistic system optimisation, targeting areas with greater potential for savings.
By partnering with Spirax Sarco and leveraging our Advance Consulting expertise, you can achieve meaningful reductions in fuel consumption and emissions—without risking the integrity of your system.
Ready to Explore Your Options?
Reducing your boiler pressure may seem like a quick win, but with Spirax Sarco, you can uncover more effective ways to optimise your steam system. Contact us today to learn how our tailored solutions can help you achieve your energy efficiency and sustainability goals—without compromise.
Let’s optimise your steam system for a better future.
Process managers could be making improvements to increase efficiency and product quality by paying closer attention to the specification of controls systems used within their facilities – that’s the current message from Spirax Sarco’s National Controls Specialist, Darren Silverthorn.
Process, energy, and maintenance managers looking to maximise safety, efficiency, and productivity, are being urged to take a proactive approach to plant management by including wireless steam trap monitoring within their proactive maintenance regime.
Believe it or not, you can make this a reality through your choice of control valve. You will already know that accurate temperature and pressure control maintains process efficiency, which makes control valves an invaluable part of any steam system. So what should you be looking for when sourcing an efficient control valve?
Implementing an effective steam trap management plan, doesn’t need to be complicated. Lowering Carbon output, increased production and energy savings are all benefits you could achieve from regular management.
Industrial steam specialist, Spirax Sarco Limited, headquartered in Gloucestershire, has begun machining a critical component part for use in the UCL-Ventura breathing aid, a Continuous Positive Airway Pressure (CPAP) device that is being used to provide potentially life-saving oxygen to patients affected by COVID-19.
Measures the conductivity of a liquid, degree of purity is established. The amount of dissolved solids in boiler water can be directly related to its conductivity level.