Description of water tube boilers including operation, types and benefits; also, a brief synopsis on how they are applied to combined heat and power generation.
Water-tube boilers differ from shell type boilers in that the water is circulated inside the tubes, with the heat source surrounding them. Referring back to the equation for hoop stress (Equation 3.2.1), it is easy to see that because the tube diameter is significantly smaller, much higher pressures can be tolerated for the same stress.
Water-tube boilers are used in power station applications that require:
However, water-tube boilers are also manufactured in sizes to compete with shell boilers.
Small water-tube boilers may be manufactured and assembled into a single unit, just like packaged shell boilers, whereas large units are usually manufactured in sections for assembly on site.
Many water-tube boilers operate on the principle of natural water circulation (also known as ‘thermosiphoning’). This is a subject that is worth covering before looking at the different types of water-tube boilers that are available. Figure 3.3.2 helps to explain this principle:
However, when the pressure in the water-tube boiler is increased, the difference between the densities of the water and saturated steam falls, consequently less circulation occurs. To keep the same level of steam output at higher design pressures, the distance between the lower drum and the steam drum must be increased, or some means of forced circulation must be introduced.
Water-tube boiler sections
The energy from the heat source may be extracted as either radiant or convection and conduction.
The furnace or radiant section
This is an open area accommodating the flame(s) from the burner(s). If the flames were allowed to come into contact with the boiler tubes, serious erosion and finally tube failure would occur.
The walls of the furnace section are lined with finned tubes called membrane panels, which are designed to absorb the radiant heat from the flame.
This part is designed to absorb the heat from the hot gases by conduction and convection.
Large boilers may have several tube banks (also called pendants) in series, in order to gain maximum energy from the hot gases.
Water-tube boiler designation
Water-tube boilers are usually classified according to certain characteristics, see Table 3.3.1.
The following layouts work on the same principles as other water-tube boilers, and are available with capacities from 5 000 kg/h to 180 000 kg/h.
Longitudinal drum boiler
The longitudinal drum boiler was the original type of water-tube boiler that operated on the thermo-siphon principle (see Figure 3.3.5).
Cooler feedwater is fed into a drum, which is placed longitudinally above the heat source. The cooler water falls down a rear circulation header into several inclined heated tubes. As the water temperature increases as it passes up through the inclined tubes, it boils and its density decreases, therefore circulating hot water and steam up the inclined tubes into the front circulation header which feeds back to the drum. In the drum, the steam bubbles separate from the water and the steam can be taken off.
Typical capacities for longitudinal drum boilers range from 2 250 kg/h to 36 000 kg/h.
The cross drum boiler is a variant of the longitudinal drum boiler in that the drum is placed cross ways to the heat source as shown in Figure 3.3.6. The cross drum operates on the same principle as the longitudinal drum except that it achieves a more uniform temperature across the drum. However it does risk damage due to faulty circulation at high steam loads; if the upper tubes become dry, they can overheat and eventually fail.
The cross drum boiler also has the added advantage of being able to serve a larger number of inclined tubes due to its cross ways position.
Typical capacities for a cross drum boiler range from 700 kg/h to 240 000 kg/h.
A further development of the water-tube boiler is the bent tube or Stirling boiler shown inFigure 3.3.7. Again this operates on the principle of the temperature and density of water, but utilises four drums in the following configuration.
Cooler feedwater enters the left upper drum, where it falls due to greater density, towards the lower, or water drum. The water within the water drum, and the connecting pipes to the other two upper drums, are heated, and the steam bubbles produced rise into the upper drums where the steam is then taken off.
The bent tube or Stirling boiler allows for a large surface heat transfer area, as well as promoting natural water circulation.
Advantages of water-tube boilers:
Disadvantages of water-tube boilers:
The water-tube boilers described above are usually of a large capacity. However, small, special purpose, smaller waste heat boilers to be used in conjunction with land based gas turbine plants are in increasing demand.
Several types of steam generating land based gas turbine plant are used:
These systems direct the hot exhaust gases from a gas turbine (approximately 500°C) through a boiler, where saturated steam is generated and used as a plant utility.
Typical applications for these systems are on plant or sites where the demands for electricity and steam are in step and of proportions which can be matched to a CHP system.
Efficiencies can reach 90%.
These are extensions to CHP systems, and the saturated steam is taken through a superheater to produce superheated steam. The superheater may be separately fired because of the comparatively low temperature of the gas turbine exhaust. The superheated steam produced is directed to steam turbines which drive additional alternators, and generate electricity.
The turndown ratio of these plants is poor, because of the need for the turbine to rotate at a speed synchronised to the electrical frequency. This means that it is only practical to run these plants at full-load, providing the base load of steam to the plant.
Because of the relatively low temperature of the gas turbine exhaust, compared to the burner flame in a conventional boiler, a much greater boiler heat transfer area is required for a given heat load. Also, there is no need to provide accommodation for burners. For these reasons, water-tube boilers tend to provide a better and more compact solution. Because efficiency is a major factor with CHP decision-makers, the design of these boilers may well incorporate an economiser (feedwater heater).
If the plant is ‘combined cycle’ the design may also include a superheater. However, the relatively low temperatures may mean that additional burners are required to bring the steam up to the specification required for the steam turbines.