Today is the perfect time to be proactive and consider preventative maintenance. The heating season is very near. Don’t wait until the temperatures are freezing to get your steam plant ready. Being proactive and making preparations now can prevent system downtime and unplanned maintenance. The questions and answers below will help you understand why now is indeed, the time to prepare.
Is your boiler ready to operate at high capacity?
During the winter months your boiler will be operating at a stronger capacity than it does during other months of the year. Boiler failure can effect steam pressure and process equipment and result in poor performance of the steam system overall. Steam system failure can also be a result, and can lead to unplanned downtime and lost production. Be proactive now and contact your local boiler service technician for a boiler tune up.
Is your steam system producing good quality steam?
In order for your plant to operate at its peak performance, steam should be delivered in the correct quantity, and at the correct pressure and temperature. It should be clean, dry, and free from air and other non-condensable gases. Good quality steam will ensure that you achieve the compliance and safety standards that are required for many processes and good quality steam can cut your energy costs, improve productivity and product quality, as well as reduce maintenance workload. If you are unsure of your steam quality, contact your local Spirax Sarco representative today about a steam system assessment.
Are your pressure reducing valves working properly?
Well-designed steam systems produce clean dry steam for delivery at high pressure. Lower pressure steam is usually needed at the point of use. Effective control demands an automatic pressure reducing valve that can reduce steam pressure accurately and reliably.
Watch this video to troubleshoot your pressure reducing valves. Need help with this task or are you thinking that your valves need repair? Our Spirax Sarco steam experts are available to assist.
Are your steam pipes and steam equipment well insulated?
The steam in your system piping gives up energy to the areas that surround the pipe. As it gives up its energy, condensate is formed in the pipe and must be removed to ensure good steam quality is achieved. When the temperature begins to fall and the area around pipes becomes cold, energy will be wasted if your pipes are poorly insulated. Like steam pipes, important piping components such as pressure reducing valves, strainers, mechanical steam traps, control and isolation valve bodies, and condensate pump receivers can waste energy if not insulated. Removable insulation jackets are an effective way to insulate piping components. A well-insulated steam system will ensure that wasted energy will be minimal and will also result in less steam being produced by the boiler.
If your steam system has bare pipes and flanges, damaged or wet insulation, uninsulated steam components, and uninsulated valve bodies, rest assured that Spirax Sarco can help. Get in touch with your local steam expert for assistance in correcting these issues.
Are your steam traps working properly?
It is very important to maintain your steam trap population and keep it in good order. A healthy steam trap population allows condensate to be removed from the steam system effectively which means that process efficiency can be optimized, equipment is protected and the condensate can be re-used. Good steam trap management ensures good steam quality, improved safety, and energy savings in your steam system. It also results in less chance of damage from issues like waterhammer, corrosion, erosion, and freezing.
Below are some points to consider about steam traps and getting your system prepared for winter.
If you’ve answered 'yes' to the questions above and need a bit of advice, our expert engineers are available and ready to help. Get in touch today.
This podcast series is a “must listen” if you’re interested in improving sustainability, increasing energy savings, understanding condensate recovery and why it’s beneficial, steam quality importance, best practices for steam system design in your industry, and many other useful steam engineering topics.
Learn about the principles of steam engineering and heat transfer, covering all aspects of steam and condensate systems; from the boiler house and steam distribution system; through the condensate recovery system and returning to the boiler.
Spirax Sarco’s steam experts have devised this complimentary eguide to help you understand the benefits and solutions to effective steam trap management. We are focused on helping our customers to improve process efficiency, increase production output, and achieve energy savings, and we know the importance of effective steam trap management in achieving this. Download the guide today!
In this webinar recording Spirax Sarco steam experts discussed how each steam trap application has its own set of particular requirements. You will learn how selecting the right steam trap for your application could have a significant, positive impact on your process, potentially improving efficiency, reducing energy costs, and giving you a safer working environment.
Did you know irrespective of the type or brand, steam traps are recognized as a potential source for significant energy loss?
In this recorded webinar Spirax Sarco steam experts, Jennifer Carlino and Jarrett Dozier discuss steam trap maintenance programs and how they can identify steam leaks with the goal of targeting and prioritizing areas of the plant, which with further investigation, could lead to greater savings and improvements. In addition, our experts will identify opportunities to reduce total cost of ownership and share best practices for steam applications.
Condensate is a valuable resource. Find out why recovering and recycling even small quantities can be economically beneficial.
When it comes to product choice, it’s all here.