“Leaking steam has a huge impact on customers’ process and profits. Spira-trol™ Steam-Tight targets the source of the problem, eliminating leaking steam control valves from the plant.”Chris Glass, Spirax Sarco Product Manager
Spirax Sarco, the global leader in steam system engineering and management has expanded its product line to include the new Spira-trol™ Steam-Tight control valve, helping customers maximize output, minimize downtime, and improve product quality. This exciting new product release has a full peak class VI shutoff double life seat, increasing the life span of the steam plant, simplifying plant maintenance throughout the life cycle of operation, and driving down the total cost of ownership for customers in the food, beverage, oil, gas, chemical, and healthcare industries.
“Leaking steam has a huge impact on customers’ process and profits. Spira-trol™ Steam-Tight targets the source of the problem, eliminating leaking steam control valves from the plant.” said Chris Glass, Spirax Sarco Product Manager.
According to Glass, the Spira-trol™ Steam-Tight control valve has a low impact on maintenance because the valve is not required to be removed from the line and requires no special tools. This new product solution is available in sizes half inch to 4 inch and comes in SG Iron, Carbon Steel, and Stainless Steel. It’s suitable for steam pressures to 275 psig, steam temperatures to 428°F, and comes with a 3 year warranty.
Watch this video now and discover how Spira-trol Steam-Tight works
Information about the Spira-trol™ Steam-Tight control valve is just a mouse click away