Leaking steam has a huge impact on customers’ process and profits. Spira-trol™ Steam-Tight targets the source of the problem, eliminating leaking steam control valves from the plant. The addition of Spira-trol™ Steam-Tight to the Quick Ship program will help customers maximize output, minimize downtime, and improve product quality.Chris Rossi, Spirax Sarco Product Manager
Spirax Sarco US announces the addition of Steam-Tight PEEK seats to its Spira-trol™ line of modular control valves, which ship in four days or less through the company’s Quick Ship program. The valves leave the factory preconfigured for the intended application, simplifying installation and minimizing customer downtime.
“Leaking steam has a huge impact on customers’ process and profits. Spira-trol™ Steam-Tight targets the source of the problem, eliminating leaking steam control valves from the plant. The addition of Spira-trol™ Steam-Tight to the Quick Ship program will help customers maximize output, minimize downtime, and improve product quality.” said Chris Rossi, Spirax Sarco Product Manager.
According to Rossi, the Spira-trol™ Steam-Tight has a full PEEK class VI shutoff double life seat, increasing the life span of the steam plant, simplifying plant maintenance throughout the life cycle of operation, and driving down the total cost of ownership for customers in the food, beverage, chemical, and healthcare industries. The Spira-trol™ Steam-Tight control valve has a low impact on maintenance because the valve is not required to be removed from the line and requires no special tools. This product solution is available in sizes half-inch to 4 inch and comes in SG Iron, Carbon Steel, and Stainless Steel. It's suitable for steam pressures up to 275 psig, steam temperatures up to 428°F, and comes with a 3 year warranty.
More information about the Spira-trol control valve Quick Ship Program is a mouse-click away.