There are many good reasons for reducing (and sometimes maintaining) steam pressure. This tutorial details common applications for direct operating, pilot operated, pneumatic, electric and electropneumatic pressure control systems, including the advantages and disadvantages of each different control method.
Description
With this self-acting type of pressure controller, the downstream (control) pressure is balanced (via a bellows) against a spring force.
Advantages:
Disadvantages:
Applications:
Non-critical, moderate load applications with constant running flowrates, for example:
Points to note:
With this self-acting type of pressure controller, the downstream (control) pressure is balanced (via a diaphragm) against a spring force.
Advantages:
Disadvantage:
Application:
Points to note:
Description
These have a more complex self-acting design, and operate by sensing the downstream pressure via a pilot valve, which in turn operates the main valve.
The effect is a very narrow proportional band, typically less than 200 kPa.
This, together with low hysterisis, results in very tight and repeatable control of pressure, even with widely varying flowrates.
Advantages:
Disadvantages:
Application:
Points to note:
Description
These control systems may include:
Advantages:
Disadvantages:
Application:
A system which requires accurate and consistent pressure control, and installations which have variable and high flowrates and/or variable or high upstream pressure. For example: autoclaves, highly rated plant such as large heat exchangers and calorifiers.
Points to note:
Description
These control systems may include:
Advantages:
Disadvantages:
Application:
A system which requires accurate and consistent pressure control, and installations which have variable and high flowrates and/or variable or high upstream pressure, including autoclaves, highly rated plant such as large heat exchangers and calorifiers, and main plant pressure reducing stations.
Points to note:
Description
These control systems may include:
Advantages:
Disadvantages:
Application:
Points to note:
Description
Pressure reducing stations may be configured as shown below for one of two reasons:
Points to note:
The valves selected for this type of application will require narrow proportional bands (such as pilot operated pressure reducing valves or electropneumatic control systems) to avoid the downstream pressure dropping too much at high flow rates.
A pressure reducing station may be configured in this manner if the ratio between the upstream and downstream pressure is very high, and the control systems selected have a low turndown ability. 10:1 is recommended as a practical maximum pressure ratio for this type of reducing valve.
Consider the need to drop pressure from 25 bar g to 1 bar g. The primary reducing valve might reduce pressure from 25 bar g to 5 bar g, which constitutes a pressure ratio of 5:1. The secondary reducing valve would drop pressure from 5 bar g to 1 bar g, also 5:1. Both valves in series provide a pressure ratio of 25:1.
It is important to check the allowable pressure turndown ratio on the selected reducing valve, this may be 10:1 on a self-acting valve, but can be much higher on electrically or pneumatically operated valves. Be aware that high pressure drops might have a tendency to create high noise levels. Refer to Module 6.4 for further details.
The trapping point between the two reducing valves (Figure 8.1.8) is to stop a build up of condensate under no-load conditions. If this were not fitted, radiation losses would cause condensate to fill the connecting pipe, which would cause waterhammer the next time the load increased.
Desuperheating is the process by which superheated steam is either restored to its saturated state, or its superheated temperature is reduced. Further coverage of desuperheaters is given in Block 15.
The system in Figure 8.1.9 illustrates an arrangement of a pressure reducing station with a direct contact type pipeline desuperheater.
In its basic form, good quality water (typically condensate) is directed into the superheated steam flow, removing heat from the steam, causing a drop in the steam temperature.
It is impractical to reduce the steam temperature to its saturated value, as the control system is unable to differentiate between saturated steam and wet steam at the same temperature.
Because of this, the temperature is always controlled at a value higher than the relevant saturation temperature, usually at 5°C to 10°C above saturation.
For most applications, the basic system as shown in Figure 8.1.9 will work well. As the downstream pressure is maintained at a constant value by the pressure control loop, the set value on the temperature controller does not need to vary; it simply needs to be set at a temperature slightly above the corresponding saturation temperature.
However, sometimes a more complex control system is required, and is shown in Figure 8.1.10. Should there be a transient change in the superheated steam supply pressure, or a change in the water supply temperature, the required water/steam flow ratio will also need to change.
A change in the water/steam flow ratio will also be required if the downstream pressure changes, as is sometimes the case with certain industrial processes.
The system shown in Figure 8.1.10 works by having the pressure controller set at the required downstream pressure and operating the steam pressure control valve accordingly.
The 4-20 mA signal from the pressure transmitter is relayed to the pressure controller and the saturation temperature computer, from which the computer continuously calculates the saturation temperature for the downstream pressure, and transmits a 4-20 mA output signal to the temperature controller in relation to this temperature.
The temperature controller is configured to accept the 4-20 mA signal from the computer to determine its set point at 5°C to 10°C above saturation. In this way, if the downstream pressure varies due to any of the reasons mentioned above, the temperature set point will also automatically vary. This will maintain the correct water/steam ratio under all load or downstream pressure conditions.
Description
These are applications which utilise the predictable relationship between saturated steam pressure and its temperature.
Advantages:
Disadvantage:
Applications:
Points to note:
Description
In these applications the control valve will open and close to maintain a set differential pressure between two points.
Advantages:
Disadvantage:
Application:
Points to note:
A special controller or differential pressure transmitter is required to accept two inputs; one from the primary steam supply and the other from the flash vessel. In this way, the pressure differential between the flash vessel and the primary steam supply is maintained under all load conditions.
Description
The objective is to maintain the pressure upstream of the control valve. Surplussing valves are discussed in further detail in Module 7.3, ’Self-acting pressure controls and applications’.
Application:
Points to note:
Description
Where it is necessary to control two variables with one valve it is necessary to employ two separate controllers and sensors. It is always the case that the control valve accepts its control signal from the slave controller.
The slave controller is configured to accept two input signals, and its set point will change (within defined limits) depending on the electrical output signal from the master controller.
This form of control is very important where the pressure to the apparatus must be limited, despite the heat demand.
Application:
The steam heated plate heat exchanger shown in Figure 8.1.19 is heating water circulating in a secondary system. The heat exchanger has a maximum working pressure, consequently this is limited to that value in the slave controller.
In order to control the secondary water temperature, a master controller and temperature transmitter monitors the heat exchanger outflow temperature and sends a 4-20 mA signal to the slave controller, which is used to vary the slave set point, between pre-determined limits.
Points to note:
Description
The objective is to reduce steam pressure but not at the expense of overloading the available supply capacity.
Application:
The upstream pipework is a high-pressure distribution pipe possibly from a distribution manifold or steam boiler supplying plant of a non-essential nature (Figure 8.1.20). Should the demand be higher than the supply capacity, the valve closes and throttles the steam flow, maintaining the pressure in the upstream pipework.
The master controller is set at the normal expected supply pressure. If the master detects a drop in upstream pressure below its set value (due to an increase in demand) it reduces the set point in the slave controller, in proportion to pre-determined limits.
The slave closes the valve until the steam demand falls to allow the upstream pressure to re-establish to the required value. When this is achieved, the set point of the slave controller is set at its original value.
Typical settings
The output from the master controller is direct acting, that is, when the upstream pressure is at or above its proportional band, the master’s output signal is maximum at 20 mA; when at the bottom of, or below the proportional band, the control signal is minimum at 4 mA.
When the control signal is 20 mA, the slave set point is the required downstream pressure; when the signal is 4 mA, the slave set point is at a pre-determined minimum.
Consider the ‘normal’ upstream pressure to be 10 bar g, and the maximum allowable downstream pressure to be 5 bar g. The minimum allowable upstream pressure is 8.5 bar g, which means that if this pressure is reached the valve is fully shut. The minimum reduced pressure is set at 4.6 bar g.
These conditions are recorded in Table 8.1.1
Description
The main objective is to limit and regulate the temperature to a particular process, where steam is the available heat source but it cannot be used directly to heat the final product for operational reasons.
Application:
A typical application is a dairy cream pasteuriser requiring a pasteurisation temperature of 50°C. Because of the low control temperature, if steam were applied directly to the pasteurisation heat exchanger, it is possible that the relatively large amount of heat in the steam would make control difficult, causing the system temperatures to oscillate, overheating and spoiling the cream.
To overcome this problem, the system in Figure 8.1.21 shows two heat exchangers. The pasteuriser is heated by hot water supplied from the primary steam heated heat exchanger.
However, even with this arrangement, if only the master controller operated the valve, a time lag would be introduced into the system, and poor control might again be the result.
Two controllers are therefore used, working in cascade, each receiving a 4-20 mA signal from their respective temperature transmitters.
The slave controller is used to control the final temperature of the product within clearly defined limits (perhaps between 49°C and 51°C). These values are altered by the master controller relative to the product temperature such that, if the product temperature increases, the slave set point reduces in proportion.