New Standard in Steam Trap Monitoring

Simplify your maintenance routine

EcoBolt Clamped_13

In any steam system, there is one component whose importance cannot be overstated. From a simple steam and condensate loop to a complex operation, the steam trap’s role is crucial: to discharge condensate and non-condensable gases while stopping live steam from escaping.

Of course, we’re talking about the steam trap. With over 200 years of history, its impact on any steam system is huge. Today, its role is more vital than ever, as it is key to maintaining thermal process efficiency and sustainability.

The Traditional Approach to Steam Trap Maintenance

Anyone responsible for a steam system knows the importance of steam trap performance. A failed steam trap can lead to significant issues, such as unscheduled production downtime and increased energy costs.

For organisations focused on sustainability and profitability, regular steam trap surveys are considered best practise. The survey or audit frequency depends on the steam system in place.

For instance, the U.S. Department of Energy recommends the following intervals based on operating pressure:

  • High Pressure (150 psig and above): Weekly to Monthly

  • Medium Pressure (30 to 150 psig): Monthly to Quarterly

  • Low Pressure (below 30 psig): Yearly

These are recommended intervals, not mandatory standards.

U.S. Department of Energy has noted that: "In steam systems that have not been maintained for 3 to 5 years, between 15% to 30% of the installed steam traps may have failed.... " ¹
U.S. Department of Energy

While statistics on steam trap failures vary, one thing is clear: steam traps will fail, whether by remaining permanently open or closed. Estimates suggest that an average-quality steam trap could only last four years, compared to double this for higher-quality options, such as those offered by Spirax Sarco.

The Future of Steam Trap Maintenance: Remote Monitoring

The ability to remotely monitor steam traps in near real-time has existed for a while. Early solutions relied on a basic “traffic light” system, where green indicated proper operation and red signalled a problem.

Even with handheld steam trap monitoring devices, there’s a margin for error. A brief snapshot, sometimes lasting as little as 15 seconds, can be influenced by noise from surrounding equipment, leading to inaccurate readings.

While manual monitoring still has its place, Spirax Sarco's wireless steam trap monitoring solution represents an advancement in monitoring reliability. Our solution provides accurate near real-time steam trap performance insights, eliminating the guesswork that comes with periodic checks.

Spirax Sarco's wireless steam trap monitoring platform securely captures precise steam trap data and delivers actionable insights to help protect expensive equipment, prevent plant disruption, control costs and improve sustainability.

Steam traps will remain a key part of any steam system, but we can evolve how we manage them. By adopting smarter solutions like wireless steam trap monitoring, you can ensure that your connected steam traps operate at peak efficiency and avoid the limitations of manual steam trap monitoring.

Optimise your steam generation, distribution, and use with Spirax Sarco.

Enhance System Reliability, Cut Costs, and Boost Sustainability with Spirax Sarco’s Wireless Steam Trap Monitoring

Managing your steam traps doesn’t need to be a hassle. Partner with Spirax Sarco today and discover how our wireless monitoring solutions can benefit your operations.

Note:

¹: U.S. Department of Energy: Inspect and Repair Steam Traps