Looking for Spirax Sarco products and services?

Steam Distribution

Masthead background

Steam Mains and Drainage

Issues surrounding the structure, layout and operation of a steam distribution system, including condensate drain points and branch lines, the avoidance of waterhammer and the use of separators and strainers for steam conditioning.

Steam Mains and Drainage Introduction

Throughout the length of a hot steam main, an amount of heat will be transferred to the environment, and this will depend on the parameters identified in Block 2 - ‘Steam Engineering and Heat Transfer’, and brought together in Equation 2.5.1.

equation 2.5.1

With steam systems, this loss of energy represents inefficiency, and thus pipes are insulated to limit these losses. Whatever the quality or thickness of insulation, there will always be a level of heat loss, and this will cause steam to condense along the length of the main.

The effect of insulation is discussed in Module 10.5. This Module will concentrate on disposal of the inevitable condensate, which, unless removed, will accumulate and lead to problems such as corrosion, erosion, and waterhammer.

In addition, the steam will become wet as it picks up water droplets, which reduces its heat transfer potential. If water is allowed to accumulate, the overall effective cross sectional area of the pipe is reduced, and steam velocity can increase above the recommended limits.

Piping layout

It is good engineering practice that, whenever possible, the main should be installed with a fall of not less than 1:100 (1 m fall for every 100 m run), in the direction of the steam flow. This slope will ensure that gravity, as well as the flow of steam, will assist in moving the condensate towards drain points where the condensate may be safely and effectively removed (See Figure 10.3.1).

10.3.1 Typical steam main installation

Drain points

The drain point must ensure that the condensate can reach the steam trap. Careful consideration must therefore be given to the design and location of drain points.

Consideration must also be given to condensate remaining in a steam main at shutdown, when steam flow ceases. Gravity will ensure that the water (condensate) will run along sloping pipework and collect at low points in the system. Steam traps should therefore be fitted to these low points.

The amount of condensate formed in a large steam main under start-up conditions is sufficient to require the provision of drain points at intervals of 30 m to 50 m, as well as natural low points such as at the bottom of rising pipework.

In normal operation, steam may flow along the main at speeds of up to 145 km/h, dragging condensate along with it. Figure 10.3.2 shows a 15 mm drain pipe connected directly to the bottom of a main.

10.3.2 Trap pocket too small

Although the 15 mm pipe has sufficient capacity, it is unlikely to capture much of the condensate moving along the main at high speed. This arrangement will be ineffective.

A more reliable solution for the removal of condensate is shown in Figure 10.3.3. The trap line should be at least 25 to 30 mm from the bottom of the pocket for steam mains up to 100 mm, and at least 50 mm for larger mains. This allows a space below for any dirt and scale to settle.

10.3.3 Trap pocket properly sized

The bottom of the pocket may be fitted with a removable flange or blowdown valve for cleaning purposes.

Recommended drain pocket dimensions are shown in Table 10.3.1 and in Figure 10.3.4.

Table 10.3.1 Recommended drain pocket dimensions

Mains diameter - D Pocket diameter - d1 Pocket depth - d2
Up to 100 mm nb d1 = D Minimum d2 = 100 mm
125 - 200 mm nb d1 = 100 mm Minimum d2 = 150 mm
250 mm and above d1 > D / 2 Minimum d2 = D

Recomended drain pocket dimensions

Waterhammer and its effects

Waterhammer is the noise caused by slugs of condensate colliding at high velocity into pipework fittings, plant, and equipment. This has a number of implications:

  • Because the condensate velocity is higher than normal, the dissipation of kinetic energy is higher than would normally be expected.
  • Water is dense and incompressible, so the ‘cushioning’ effect experienced when gases encounter obstructions is absent.
  • The energy in the water is dissipated against the obstructions in the piping system such as valves and fittings.
10.3.5 Formation of 'solid' slug water

Indications of waterhammer include a banging noise, and perhaps movement of the pipe.

In severe cases, waterhammer may fracture pipeline equipment with almost explosive effect, with consequent loss of live steam at the fracture, leading to an extremely hazardous situation.

Good engineering design, installation and maintenance will avoid waterhammer; this is far better practice than attempting to contain it by choice of materials and pressure ratings of equipment.

Commonly, sources of waterhammer occur at the low points in the pipework (See Figure 10.3.6). Such areas are due to:

  • Sagging in the line, perhaps due to failure of supports.
  • Incorrect use of concentric reducers (see Figure 10.3.7) - Always use eccentric reducers with the flat at the bottom.
  • Incorrect strainer installation - They should be fitted with the basket on the side.
  • Inadequate drainage of steam lines.
  • Incorrect operation - Opening valves too quickly at start-up when pipes are cold.
10.3.6 Potential sources of waterhammer

To summarise, the possibility of waterhammer is minimised by:

  • Installing steam lines with a gradual fall in the direction of flow, and with drain points installed at regular intervals and at low points.
  • Installing check valves after all steam traps which would otherwise allow condensate to run back into the steam line or plant during shutdown.
  • Opening isolation valves slowly to allow any condensate which may be lying in the system to flow gently through the drain traps, before it is picked up by high velocity steam. This is especially important at start-up.
10.3.8 Branch line

Branch lines are normally much shorter than steam mains. As a general rule, therefore, provided the branch line is not more than 10 metres in length, and the pressure in the main is adequate, it is possible to size the pipe on a velocity of 25 to 40 m/s, and not to worry about the pressure drop.

Table 10.2.4 ‘Saturated steam pipeline capacities for different velocities’ in Module 10.2 will prove useful in this exercise.

Branch line connections

Branch line connections taken from the top of the main carry the driest steam (Figure 10.3.8). If connections are taken from the side, or even worse from the bottom (as in Figure 10.3.9 (a)), they can accept the condensate and debris from the steam main. The result is very wet and dirty steam reaching the equipment, which will affect performance in both the short and long term.

The valve in Figure 10.3.9 (b) should be positioned as near to the off-take as possible to minimise condensate lying in the branch line, if the plant is likely to be shutdown for any extended periods.

10.3.9 Steam take-off

Drop Leg

Low points will also occur in branch lines. The most common is a drop leg close to an isolating valve or a control valve (Figure 10.3.10). Condensate can accumulate on the upstream side of the closed valve, and then be propelled forward with the steam when the valve opens again - consequently a drain point with a steam trap set is good practice just prior to the strainer and control valve.

10.3.10 Diagram of drop leg supplying a unit heater

Rising ground and drainage

There are many occasions when a steam main must run across rising ground, or applications where the contours of the site make it impractical to lay the pipe with the 1:100 fall proposed earlier. In these situations, the condensate must be encouraged to run downhill and against the steam flow. Good practice is to size the pipe on a low steam velocity of not more than 15 m/s, to run the line at a slope of no less than 1:40, and install the drain points at not more than 15 metre intervals (see Figure 10.3.11).

The objective is to prevent the condensate film on the bottom of the pipe increasing in thickness to the point where droplets can be picked up by the steam flow.

10.3.11 Reverse gradient on steam main

Steam separators

Modern packaged steam boilers have a large evaporating capacity for their size and have limited capacity to cope with rapidly changing loads. In addition, as discussed in Block 3 ‘The Boiler House’, other circumstances, such as . . .

  • Incorrect chemical feedwater treatment and/or TDS control
  • Transient peak loads in other parts of the plant

. . . can cause priming and carryover of boiler water into the steam mains.

Separators, as shown by the cut section in Figure 10.3.12, may be installed to remove this water.

10.3.12 Cut section trhough separator

As a general rule, providing the velocities in the pipework are within reasonable limits, separators will be line sized. (Separators are discussed in detail in Module 12.5)

A separator will remove both droplets of water from pipe walls and suspended mist entrained in the steam itself. The presence and effect of waterhammer can be eradicated by fitting a separator in a steam main, and can often be less expensive than increasing the pipe size and fabricating drain pockets.

A separator is recommended before control valves and flowmeters. It is also wise to fit a separator where a steam main enters a building from outside. This will ensure that any condensate produced in the external distribution system is removed and the building always receives dry steam. This is equally important where steam usage in the building is monitored and charged for.

Strainers

When new pipework is installed, it is not uncommon for fragments of casting sand, packing, jointing, swarf, welding rods and even nuts and bolts to be accidentally deposited inside the pipe. In the case of older pipework, there will be rust, and in hard water districts, a carbonate deposit. Occasionally, pieces will break loose and pass along the pipework with the steam to rest inside a piece of steam using equipment. This may, for example, prevent a valve from opening/closing correctly. Steam using equipment may also suffer permanent damage through wiredrawing - the cutting action of high velocity steam and water passing through a partly open valve. Once wiredrawing has occurred, the valve will never give a tight shut-off, even if the dirt is removed.

It is therefore wise to fit a line-size strainer in front of every steam trap, flowmeter, reducing valve and regulating valve. The illustration shown in Figure 10.3.13 shows a cut section through a typical strainer.

10.3.13 Cut section through a Y-type strainer

Steam flows from the inlet ‘A’ through the perforated screen ‘B’ to the outlet ‘C’. While steam and water will pass readily through the screen, dirt cannot. The cap ‘D’, can be removed, allowing the screen to be withdrawn and cleaned at regular intervals. A blowdown valve can also be fitted to cap ‘D’ to facilitate regular cleaning.

Strainers can however, be a source of wet steam as previously mentioned. To avoid this situation, strainers should always be installed in steam lines with their baskets to the side.

Strainers and screen details are discussed in Module 12.4.

How to drain steam mains

Steam traps are the most effective and efficient method of draining condensate from a steam distribution system.

The steam traps selected must suit the system in terms of:

  • Pressure rating
  • Capacity
  • Suitability

Pressure rating

Pressure rating is easily dealt with; the maximum possible working pressure at the steam trap will either be known or should be established.

Capacity

Capacity, that is, the quantity of condensate to be discharged, which needs to be divided into two categories; warm-up load and running load.

Warm-up load

In the first instance, the pipework needs to be brought up to operating temperature. This can be determined by calculation, knowing the mass and specific heat of the pipework and fittings. Alternatively, Table 10.3.2 may be used.

  • The table shows the amount of condensate generated when bringing 50 m of steam main up to working temperature; 50 m being the maximum recommended distance between trapping points.
  • The values shown are in kilograms. To determine the average condensing rate, the time taken for the process must be considered. For example, if the warm-up process required 50 kg of steam, and was to take 20 minutes, then the average condensing rate would be:
equation 10.3.a
  • When using these capacities to size a steam trap, it is worth remembering that the initial pressure in the main will be little more than atmospheric when the warm-up process begins. However, the condensate loads will still generally be well within the capacity of a DN15 ‘low capacity’ steam trap. Only in rare applications at very high pressures (above 70 bar g), combined with large pipe sizes, will greater trap capacity be needed.

Running Load

Once the steam main is up to operating temperature, the rate of condensation is mainly a function of the pipe size and the quality and thickness of the insulation.

For accurate means of calculating running losses from steam mains, refer to Module 2.12 ‘Steam consumption of pipes and air heaters’. Alternatively, for quick approximations of running load, Table 10.3.3 can be used which shows typical amounts of steam condensed each hour per 50 m of insulated steam main at various pressures.

Table 10.3.2

Amount of steam condensed to warm-up 50 m of schedule 40 pipe (kg)

Note: Figures are based on an ambient temperature of 20c, and an insulation efficiency of 80%

Steam pressure bar g Steam main size (mm) -18 °C correction factor
50 65 80 100 125 150 200 250 300 350 400 450 500 600
1 5 9 11 16 22 28 44 60 79 94 123 155 182 254 1.39
2 6 10 13 19 25 33 49 69 92 108 142 179 210 296 1.35
3 7 11 14 20 25 36 54 79 101 120 156 197 232 324 1.32
4 8 12 16 22 30 39 59 83 110 131 170 215 254 353 1.29
5 8 13 17 24 33 42 63 70 119 142 185 233 275 382 1.28
6 9 13 18 25 34 43 66 93 124 147 198 242 285 396 1.27
7 9 14 18 26 35 45 68 97 128 151 197 250 294 410 1.26
8 9 14 19 27 37 47 71 101 134 158 207 261 307 428 1.25
9 10 15 20 28 38 50 74 105 139 164 216 272 320 436 1.24
10 10 16 20 29 40 51 77 109 144 171 224 282 332 463 1.24
12 10 17 22 31 42 54 84 115 152 180 236 298 350 488 1.23
14 11 17 23 32 44 57 85 120 160 189 247 311 366 510 1.22
16 12 19 24 35 47 61 91 128 172 203 265 334 393 548 1.21
18 17 23 31 45 62 84 127 187 355 305 393 492 596 708 1.21
20 17 26 35 51 71 97 148 220 302 362 465 582 712 806 1.2
25 19 29 39 56 78 108 164 243 333 400 533 642 786 978 1.19
30 21 32 41 62 86 117 179 265 364 437 571 702 859 1150 1.18
40 22 34 46 67 93 127 194 287 395 473 608 762 834 1322 1.16
50 24 37 50 73 101 139 212 214 432 518 665 834 1020 1450 1.15
60 27 41 54 79 135 181 305 445 626 752 960 1218 1480 2140 1.15
70 29 44 59 86 156 208 346 510 717 861 1100 1396 1694 2455 1.15
80 32 49 65 95 172 232 386 568 800 960 1220 1550 1890 2730 1.14
90 34 51 69 100 181 245 409 598 842 1011 1288 1635 1990 2880 1.14
100 35 54 72 106 190 257 427 628 884 1062 1355 1720 2690 3030 1.14
120 42 64 86 126 227 305 508 748 1052 1265 1610 2050 2490 3600 1.13

Table 10.3.3

Condensing rate of steam in 50 m of schedule 40 pipe - at working temperature (kg/h)

Note: Figures are based on an ambient temperature of 20c, and in insulations efficiency of 80%

Steam pressure bar g Steam main size (mm) -18 °C correction factor
50 65 80 100 125 150 200 250 300 350 400 450 500 600
1 5 5 7 9 10 13 16 19 23 25 28 31 35 41 1.54
2 5 6 8 10 12 14 18 22 26 28 32 35 39 46 1.5
3 6 7 9 11 14 16 20 25 30 32 37 40 45 54 1.48
4 7 9 10 12 16 18 23 28 33 37 42 46 51 61 1.45
5 7 9 11 13 17 20 24 30 36 40 46 49 55 66 1.43
6 8 10 11 14 18 21 26 33 39 43 49 53 59 71 1.42
7 8 10 12 15 19 23 28 35 42 46 52 56 63 76 1.41
8 9 11 14 16 20 24 30 37 44 49 57 61 68 82 1.4
9 9 11 14 17 21 25 32 39 47 52 60 64 72 88 1.39
10 10 12 15 17 21 25 33 41 49 54 62 67 75 90 1.38
12 11 13 16 18 23 26 36 45 53 59 67 73 81 97 1.38
14 12 14 17 20 26 30 39 49 58 64 73 79 93 106 1.37
16 12 15 18 23 29 34 42 52 62 68 78 85 95 114 1.36
18 14 16 19 24 30 36 44 55 66 72 82 90 100 120 1.36
20 15 17 21 25 31 37 46 58 69 76 86 94 105 125 1.35
25 15 19 23 28 35 42 52 66 78 86 97 106 119 141 1.34
30 17 21 25 31 39 47 58 73 87 96 108 118 132 157 1.33
40 20 25 30 38 46 56 70 87 104 114 130 142 158 189 1.31
50 24 29 34 44 54 65 82 102 121 133 151 165 184 220 1.29
60 27 32 39 50 62 74 95 119 140 155 177 199 222 265 1.28
70 29 35 43 56 70 82 106 133 157 173 198 222 248 296 1.27
80 34 42 51 66 81 97 126 156 187 205 234 263 293 350 1.26
90 38 46 56 72 89 106 134 171 204 224 265 287 320 284 1.26
100 41 50 61 78 96 114 149 186 220 242 277 311 347 416 1.25
120 52 63 77 99 122 145 189 236 280 308 352 395 440 527 1.22

Suitability

A mains drain trap should consider the following constraints:

  • Discharge temperature - The steam trap should discharge at, or very close to saturation temperature, unless cooling legs are used between the drain point and the trap. This means that the choice is a mechanical type trap (such as a float, inverted bucket type, or thermodynamic traps).
  • Frost damage - Where the steam main is located outside a building and there is a possibility of sub-zero ambient temperature, the thermodynamic steam trap is ideal, as it not damaged by frost. Even if the installation causes water to be left in the trap at shutdown and freezing occurs, the thermodynamic trap may be thawed out without suffering damage when brought back into use.
  • Waterhammer - In the past, on poorly laid out installations where waterhammer was a common occurrence, float traps were not always ideal due to their susceptibility to float damage. Contemporary design and manufacturing techniques now produce extremely robust units for mains drainage purposes. Float traps are certainly the first choice for proprietary separators as high capacities are readily achieved, and they are able to respond quickly to rapid load increases.

Steam traps used to drain condensate from steam mains, are shown in Figure 10.3.14. The thermostatic trap is included because it is ideal where there is no choice but to discharge condensate into a flooded return pipe.

The subject of steam trapping is dealt with in detail in the Block 11, ‘Steam Trapping’.

10.3.14 Steam traps suitable for mains drainage

Steam Leaks

Steam leaking from pipework is often ignored. Leaks can be costly in both the economic and environmental sense and therefore need prompt attention to ensure the steam system is working at its optimum efficiency with a minimum impact on the environment.

Figure 10.3.15 illustrates the steam loss for various sizes of hole at various pressures. This loss can be readily translated into a fuel saving based on the annual hours of operation.

10.3.15 Steam leakage rate through holes

Summary

Proper pipe alignment and drainage means observing a few simple rules:

  • Steam lines should be arranged to fall in the direction of flow, at not less than 100 mm per 10 metres of pipe (1:100). Steam lines rising in the direction of flow should slope at not less than 250 mm per 10 metres of pipe (1:40).
  • Steam lines should be drained at regular intervals of 30-50 m and at any low points in the system.
  • Where drainage has to be provided in straight lengths of pipe, then a large bore pocket should be used to collect condensate.
  • If strainers are to be fitted, then they should be fitted on their sides.
  • Branch connections should always be taken from the top of the main from where the driest steam is taken.
  • Separators should be considered before any piece of steam using equipment ensuring that dry steam is used.
  • Traps selected should be robust enough to avoid waterhammer damage and frost damage.